What is the min and max ODR accuracy on the MMA8451

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is the min and max ODR accuracy on the MMA8451

1,716 次查看
johncampbell
Contributor II

The typical ODR accuracy is stated in Table 2 of the datasheet as +- 2%. This is at 25 C.

There are no minimum or maximum values in the datasheet.

What tolerance over temperature could be expected?

regards johnc

0 项奖励
回复
2 回复数

1,361 次查看
johncampbell
Contributor II

Thanks for your prompt response. Answers my question.

regards johnc

0 项奖励
回复

1,361 次查看
reyes
NXP TechSupport
NXP TechSupport

Dear johnc,

This is actually not a typical value, this could be seen like: MIN = -2% and MAX = +2%

The total accuracy variations should not change more than this +/-2%

Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复