What is the main reason of that the MMA865x has two interrupt outputs?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the main reason of that the MMA865x has two interrupt outputs?

Jump to solution
1,728 Views
hjlim
Contributor II

MMA865x has two interrupt pins.

Are there special cases that the user should use both channel?

Or is it just for convenience?

Labels (1)
1 Solution
1,630 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi HJ,

One interrupt pin is typically used to indicate data-ready for processor synchronization and the second one for any of the embedded functions such as any-motion (slope) detection for wake-up, tap sensing for tap-sensitive user interface control, orientation change recognition for portrait or landscape switching, low-g/high-g detection for shock and free-fall detection, or no-motion for power saving. All these embedded interrupt functions allow for overall power savings relieving the host processor from continuously polling data.


Regards,

Tomas


PS: If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.

View solution in original post

0 Kudos
Reply
1 Reply
1,631 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi HJ,

One interrupt pin is typically used to indicate data-ready for processor synchronization and the second one for any of the embedded functions such as any-motion (slope) detection for wake-up, tap sensing for tap-sensitive user interface control, orientation change recognition for portrait or landscape switching, low-g/high-g detection for shock and free-fall detection, or no-motion for power saving. All these embedded interrupt functions allow for overall power savings relieving the host processor from continuously polling data.


Regards,

Tomas


PS: If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.

0 Kudos
Reply