What are the pin assignments for the connector board that connects the Multilink programmer to the TPMS Emitter (Model FXTH870912)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What are the pin assignments for the connector board that connects the Multilink programmer to the TPMS Emitter (Model FXTH870912)?

Jump to solution
3,413 Views
alissaj558
Contributor I

I am trying to install CodeWarrior 10.6 for TPMS, and for the hardware part of the programming, there needs to be a connector board to connect the Multilink programmer to the TPMS Emitter. What are the pin assignments for the connector board?

I have the TMPS Emitter Model FXTH870912. Thanks!

0 Kudos
Reply
1 Solution
3,175 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Alissa,

P&E’s USB Multilink Universal -> TPMS emitter

BKGD (pin #1) -> BKGD (J20-1)

GND (pin #2) -> GND (J20-4)

RESET (pin #4) -> RESET (J20-2)

VDD (pin #6) -> VDD (J20-3)

Regards,

Tomas

View solution in original post

4 Replies
3,169 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Alissa,

You can find a photo showing how to connect a P&E’s USB Multilink Universal to the TPMS emiiter via a small connector in the Installing and using CW 10.6 for TPMS applications document, on page 15. More details about pin assignment gives the attached file.

If you need more information, please let me know.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

0 Kudos
Reply
3,169 Views
alissaj558
Contributor I

Thanks! I saw the image, but if I do not have a connector board, do you have the pin assignments so that I can just connect the devices with free-floating wires?

0 Kudos
Reply
3,176 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Alissa,

P&E’s USB Multilink Universal -> TPMS emitter

BKGD (pin #1) -> BKGD (J20-1)

GND (pin #2) -> GND (J20-4)

RESET (pin #4) -> RESET (J20-2)

VDD (pin #6) -> VDD (J20-3)

Regards,

Tomas

3,169 Views
alissaj558
Contributor I

Thank you!

0 Kudos
Reply