What are the pin assignments for the connector board that connects the Multilink programmer to the TPMS Emitter (Model FXTH870912)?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What are the pin assignments for the connector board that connects the Multilink programmer to the TPMS Emitter (Model FXTH870912)?

ソリューションへジャンプ
3,417件の閲覧回数
alissaj558
Contributor I

I am trying to install CodeWarrior 10.6 for TPMS, and for the hardware part of the programming, there needs to be a connector board to connect the Multilink programmer to the TPMS Emitter. What are the pin assignments for the connector board?

I have the TMPS Emitter Model FXTH870912. Thanks!

0 件の賞賛
返信
1 解決策
3,179件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Alissa,

P&E’s USB Multilink Universal -> TPMS emitter

BKGD (pin #1) -> BKGD (J20-1)

GND (pin #2) -> GND (J20-4)

RESET (pin #4) -> RESET (J20-2)

VDD (pin #6) -> VDD (J20-3)

Regards,

Tomas

元の投稿で解決策を見る

4 返答(返信)
3,173件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Alissa,

You can find a photo showing how to connect a P&E’s USB Multilink Universal to the TPMS emiiter via a small connector in the Installing and using CW 10.6 for TPMS applications document, on page 15. More details about pin assignment gives the attached file.

If you need more information, please let me know.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

0 件の賞賛
返信
3,173件の閲覧回数
alissaj558
Contributor I

Thanks! I saw the image, but if I do not have a connector board, do you have the pin assignments so that I can just connect the devices with free-floating wires?

0 件の賞賛
返信
3,180件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Alissa,

P&E’s USB Multilink Universal -> TPMS emitter

BKGD (pin #1) -> BKGD (J20-1)

GND (pin #2) -> GND (J20-4)

RESET (pin #4) -> RESET (J20-2)

VDD (pin #6) -> VDD (J20-3)

Regards,

Tomas

3,173件の閲覧回数
alissaj558
Contributor I

Thank you!

0 件の賞賛
返信