Water Pressure Sensors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Water Pressure Sensors

1,850件の閲覧回数
davidwright
Contributor I

Can the MPXM2010GS sensor be used to measure water pressure directly (ie. have the pressure spigot immersed in water with the rest of the sensor in air)? If not, is there a freescale sensor that could be used for this?

Thanks,

David

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,462件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi David,

Freescale pressure sensors are not manufactured to be submerged in water. However, the MPXM2010GS can be used to measure tank levels by using the column of air method. The sensor will read the change in pressure in the column of air as the tank fills or empties.

AN1950 - Water Level Monitoring:

http://www.freescale.com/files/sensors/doc/app_note/AN1950.pdf

AN1516 - Liquid Level Control Using a Pressure Sensor:

http://www.freescale.com/files/sensors/doc/app_note/AN1516.pdf

 

AN3728 - Media Compatibility for IPS PRT Pressure Sensors:

http://www.freescale.com/files/sensors/doc/app_note/AN3728.pdf

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

0 件の賞賛
返信