Vref pin on TJA1050T/VM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Vref pin on TJA1050T/VM

1,983 次查看
paulschoenke
Contributor III

Hello:

I'm looking for more information on the purpose and recommended termination of the Vref pin on the TJA1050T/VM device:

http://cache.nxp.com/documents/data_sheet/TJA1050.pdf?pspll=1

I don't see much information in the datasheet.

Any feedback or input is welcomed and appreciated!

Thanks again!

Paul

0 项奖励
回复
2 回复数

1,723 次查看
dietmarschmid
NXP Employee
NXP Employee

Hello Paul,

the Vref pin is to stablize common mode signal in network when used.

It is a voltage source pin and can be left open if not used.

Dietmar Schmid

FAE IVNProducts

0 项奖励
回复

1,723 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Paul,

Sorry for such a late response. I am asking our device group to comment on this and will update this thread when I get their feedback.

Regards,

Tomas

0 项奖励
回复