Vref of VSENSE block in MM9Z1_638

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Vref of VSENSE block in MM9Z1_638

ソリューションへジャンプ
1,882件の閲覧回数
shlee8467
Contributor I

Hi.

I cannot find Vref value of VSENSE block in its datasheet.

So, I tryed to calculate the Vref by comparing the analog input voltage with the ADC value.

But it changed depending on the input voltage such as 1.6321v, 1.6430v 1.649v and the value looks strange.

I have to use PTB0~PTB3 port.

Please let me know how I can calculate the correct voltage with  or without Vref.

Thanks,

ラベル(1)
0 件の賞賛
返信
1 解決策
1,748件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Seunghwan,

There is no need to know the Vref value of VSENSE.

 

The measured selected (based on VSSEL and VSEx bits of the GPIO_VSENSE register) voltage can be calculated as follows:

1. VSENSEx: V = ACQ_VOLT[15:0] x VSxRO

pastedImage_29.png

2. PTBx: V = ACQ_VOLT[15:0] x PTB0-4VRES

pastedImage_28.png

 

Best regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,749件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Seunghwan,

There is no need to know the Vref value of VSENSE.

 

The measured selected (based on VSSEL and VSEx bits of the GPIO_VSENSE register) voltage can be calculated as follows:

1. VSENSEx: V = ACQ_VOLT[15:0] x VSxRO

pastedImage_29.png

2. PTBx: V = ACQ_VOLT[15:0] x PTB0-4VRES

pastedImage_28.png

 

Best regards,

Tomas

0 件の賞賛
返信
1,748件の閲覧回数
shlee8467
Contributor I

I really appreciate it. Tomas.

0 件の賞賛
返信