Voltage input detection in NHS3152

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Voltage input detection in NHS3152

1,202 Views
younggeun
Contributor I

Hello,

I want to detect the voltage signals (potential), which changes in amplitude of about 40 uV (microvolt).

Will it be possible by using NHS3152 chip?

If possible, What is the possible additional requirement for the detection?

Thanks.

Young-Geun 

0 Kudos
Reply
1 Reply

1,113 Views
driesmoors
NXP Employee
NXP Employee

Hi,

Without knowing details: it will be a challenge. Our ADC's resolution is not high enough to detect these small differences. An amplifier may solve that, but can create new obstacles. It also depends a.o. on the region the measurements are supposed to be in.

The NHS3152 IC is targeting therapy adherence monitoring and logging use cases, where it can detect and track pill intakes. It is less suited as a general purpose ADC.

KR,
Dries.

0 Kudos
Reply