Using MMA8452Q For tilt alarm detection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using MMA8452Q For tilt alarm detection

1,259 次查看
mat66mat
Contributor I

Hello ALL,

My project is to detect an angle of about +/- 40 ° relative to an initial position .

I am a newbie in accelerometer domain and the concepts covered in the data sheet are not very clear in my mind

I'll try to ask simple questions have simple answers

1°) Is it possible to do that with MMA8452Q ?

2°) Is there an application note that clearly explains the implementation of my project with the MMA8452Q ?

thank you very much

Sincerely

Jérôme.

标签 (1)
0 项奖励
回复
1 回复

1,026 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi,

1) Yes, the MMA8452Q have an embedded orientation detection feature that can be used for a Tilt alarm detection.

2) Yes, there are some documents that can help you with this application:

  1. 2.1) AN4068 “Embedded Orientation Detection Using the MMA8451, 2, 3Q”
  2. 2.2) AN3461 “Tilt Sensing Using Three-Axis Accelerometer”

Additionally, if a +/- 45° angle detection can work for your application, I would like to recommend you to use the MMA8491Q, this accelerometer device as a 45° Tilt Sensor, it offers extreme ease of implementation by using a single line output per axis.

Have a great day,
Jose Reyes

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复