USING Pressure sensor MPXV7002GC6U can this sensor SMT soldered and be cleaned in a high aquious cleaner?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USING Pressure sensor MPXV7002GC6U can this sensor SMT soldered and be cleaned in a high aquious cleaner?

1,416件の閲覧回数
johnshandrow
Contributor I

SING Pressure sensor MPXV7002GC6U can this sensor SMT soldered and be cleaned in a high aquious cleaner?

0 件の賞賛
返信
1 返信

1,214件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi John,

Unfortunately, any cleaner that that enters the sensor pressure opening(s) may have adverse effects on the device.

So, sealing the access hole(s) on the part with kapton tape is absolutely recommended. You can plug also the sensors with a cap before cleaning. If apply, the small vent on the back of the sensor should be cover with kapton tape as well during the cleaning process.

Caps can be found via the following supplier: http://www.stockcap.com/products.asp

And just to let you know, ultrasonic cleaning is not recommended as the frequencies can damage wire bond interconnections.

Many customers have gone to no clean operations or spray clean in a direction where the spray is not directly going into the sensor hole.

You can find more details about this in the following link which will send you to a thread in the Freescale Communities: https://community.freescale.com/thread/307192

Have a great day,
Jose Reyes

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信