I want to read a real-time signal by NHS3152 NFC chip, through the current-to-digital converter.
What is the time resolution (from one data point to the next data point.. maybe the sampling rate?) of the chip?
I expect to measure body signals with a time resolution of sub-millisecond.
Young-Geun
Hi Young-Geun,
I think you are referring to the sample rate/integration time, which is supported from 10ms to 400ms. Please refer to the following for more details.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------