The differential pressure sensor MP3V5004DP CASE 1351 has two pin layouts listed on page 8 of the datasheet. Does it use "Style 1" or "Style 2"?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The differential pressure sensor MP3V5004DP CASE 1351 has two pin layouts listed on page 8 of the datasheet. Does it use "Style 1" or "Style 2"?

664 Views
xylosedai
Contributor I

http://cache.freescale.com/files/sensors/doc/data_sheet/MP3V5004G.pdf 

^datasheet to this part series

Thanks for any help!

Labels (1)
0 Kudos
Reply
1 Reply

444 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

The difference between style 1 and style 2 in the package dimensions is due to the two main families of pressure sensors NXP offers.

Style 1 is usually applicable for all MPXx10, MPXx53 and MPXx2000-series SOP Type package pressure sensors featuring differential outputs (For compensated and un-compensated pressure sensor families).

Style 2 is applicable for all MPXx4000-series, MPXx5000-series, MPXx6000-series, MPXx7000-series integrated devices in surface mount packages featuring single ended outputs (Integrated type pressure sensor families).

 

For this specific case using the MP3V5004DP, you should use “Style 2” pinout as mentioned in Figure 1 on page 3 of the MP3V5004DP datasheet.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply