Temperature compensation for MMA8452

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Temperature compensation for MMA8452

ソリューションへジャンプ
1,163件の閲覧回数
looooooost
Contributor II

So a pretty vague question: Is there a specific way to temperature compensate for the MMA8452 accelerometer? Is there an application note for it?

Do you offer any chips with a temperature sensor embedded?

 

thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
1,145件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Michael,

 

There is no specific way nor application note regarding the temperature compensation.

 

Usually no temperature calibration is needed, the zero-g level (offset) changes typically within ±0.15 mg/°C. If this represent a problem for your application, you can perform a simple two point calibration at two temperatures to compensate the TCOff.

 

Best regards,

Tomas

元の投稿で解決策を見る

1 返信
1,146件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Michael,

 

There is no specific way nor application note regarding the temperature compensation.

 

Usually no temperature calibration is needed, the zero-g level (offset) changes typically within ±0.15 mg/°C. If this represent a problem for your application, you can perform a simple two point calibration at two temperatures to compensate the TCOff.

 

Best regards,

Tomas