Dear Expert,
Now a cold storage control project used the S12ZVC MCU . It is also required the touch sensing UI .
I want to know is there possible to migrate the TSS library to S12ZVC ?
If it can't be migrated, please recommend a industrial or automotive grade MCU. The MCU must has CAN and ADC (best if the ADC there is program gain control).
Best Regards,
Kiger
已解决! 转到解答。
Dear Kiger,
The TSS is no longer recommended for new designs and there are no plans to add support for S12ZVC devices. There is a new software library – the NXP Touch Software supporting most of the Kinetis MCUs. The Kinetis E series might be a good choice, but the TSI module is available only on the KE1xZ which does not have the CAN module. So I would recommend considering our standalone touch/promixity sensors which can be connected to the S12ZVC through the I2C.
I hope it helps.
Best regards,
Tomas
PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.
Dear Kiger,
The TSS is no longer recommended for new designs and there are no plans to add support for S12ZVC devices. There is a new software library – the NXP Touch Software supporting most of the Kinetis MCUs. The Kinetis E series might be a good choice, but the TSI module is available only on the KE1xZ which does not have the CAN module. So I would recommend considering our standalone touch/promixity sensors which can be connected to the S12ZVC through the I2C.
I hope it helps.
Best regards,
Tomas
PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.