TPMS waterproof

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TPMS waterproof

1,363件の閲覧回数
tiago_silva
Contributor I

Hi, 

We intend to use the FXTH871xD, Tire Pressure Monitor
Sensor, in our project. But we work with tires filled with water, to increase the traction of a tractor. My question is, after a properly resin process, can the pressure port be in direct touch with water under pressure?

Thanks, Tiago MS#

ラベル(1)
タグ(2)
3 返答(返信)

1,173件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Tiago,

Thanks for your interest in NXP's TMPS!

I need to discuss it with the product group and should have an answer tomorrow or beginning of next week.

Best regards,

Tomas

1,173件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Tiago,

Here is the answer from our product group:

No, the gel is not 100% hermetic, and therefore over some time, a few weeks at 1500kPa, water molecules can be forced under pressure into the gel and eventually reside near the wirebonds of the Pcell, or near the top surface of the MCU.  In these cases, the dielectric constant of the water allows capacitance changes of the sensitive transducer interface circuits.  This new capacitance results in offset and/or sensitivity shifts to the calibration.  Since there is no reference for the SW to compare, the application will not recognize the shift as artificial, and instead treat as a real pressure change.  It is possible the shift can be out of tolerances.

The module should be designed in such a way that it maintains separation from the sensor to the water, and the separation methods must allow access to the pressure.

Best regards,

Tomas

1,173件の閲覧回数
tiago_silva
Contributor I

Thanks, Tomas. 

I appreciate your help. I will think in how to protect the pressure gate from the water without block the pressure...  

Best regards,

Tiago

0 件の賞賛