TPMS (Tire Pressure Monitoring System)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TPMS (Tire Pressure Monitoring System)

908 次查看
sadur
Contributor I

Hello all,

I'm currently working on "Tire Pressure Monitoring System". I did some search and found NTM88 series which is  perfect. This sensor has range of 90kPa-1518kPa. That mean is also 13psi-220psi. But I need to measure high pressure. Is there any chance that you have high range TPMS over 1600kPa. At least 300-350psi maybe.

And also I need to evaluation board

I have one more question:

Do you have evaluation board for NTM88 series.

Thanks in advance.

标签 (1)
0 项奖励
回复
3 回复数

898 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Salih,

Thank you for your interest in NXP’s TPMS solutions.

At this time, we do not offer TPMS sensors that support pressure ranges beyond 1518 kPa (220 psi). The NTM88K series is our highest-range TPMS solution, with an operating pressure range up to 1518 kPa.

For applications requiring higher pressure monitoring (such as 300 to 350 psi), you may need to explore specialized or industrial-grade TPMS solutions from other vendors.

BRs, Tomas

0 项奖励
回复

886 次查看
sadur
Contributor I
I get it. Thank you.
I had one more question but you didn't see that probably. No problem.
"Do you have evaluation board for NTM88 series?" Because at the beginning I chose FXTH87 but these sensors are not manufactured anymore. FXTH87 just has a evaluation board but no manufactured chips I think. It means it is not sustainable. So, If I draw a schematic what is your suggest to me?
Do I draw a schematic from FXTH87 or NTM88?

0 项奖励
回复

867 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Salih,

NTM88 series TPMS evaluation boards are not sold via NXP website or distributors. They are provided free of charge by NXP TPMS Application team. In order to ask for the EVB, please create a standard support ticket with the following information included:

- Brief description of your application, estimated volume and start of production.
- Desired pressure (930kPa, 1100kPa or 1518kPa) and desired frequency.
- Name, address and phone number of the person who will receive the evaluation board + VAT number of the company.

BRs, Tomas

0 项奖励
回复