Support for MMA8450 in MMA845X driver?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Support for MMA8450 in MMA845X driver?

Jump to solution
1,607 Views
Xavier
Contributor III

I need to add MMA8450 support in MMA845X official driver. Is there any patch or something to do that? Zhang Jiejing seemed to write the driver I need...

[lm-sensors] [PATCH] hwmod: sensors: mma845x gravity sensor chips

Labels (1)
0 Kudos
Reply
1 Solution
1,443 Views
Xavier
Contributor III

Since I2C driver structures were pretty much the same I injected MMA8450 driver code into MMA845X driver thanks to a if statement after having identified the chip.

View solution in original post

0 Kudos
Reply
1 Reply
1,444 Views
Xavier
Contributor III

Since I2C driver structures were pretty much the same I injected MMA8450 driver code into MMA845X driver thanks to a if statement after having identified the chip.

0 Kudos
Reply