Special receiver is needed for FXTH87?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Special receiver is needed for FXTH87?

981 Views
王亚萍
Contributor I

I try to use CC1101 as the receiver for FXTH87, but failed. But I check the datagrame ,freq, datarate, it can be matched.

Why? the hardware not match?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

664 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Yaping Wang,

Is not that the FXTH87 needs a special receiver, is just that it look like the CC1101 is a transceiver, not a receiver.

Personally, I would recommend you to use the Freescale KW01 as the receiver for the FXTH87 instead.

The application note AN5136 is a guideline about how to set the KW01 as the receiver for the FXTH87. I would recommend you to take a look at this document.


Have a great day,
Jose Reyes

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply