Smart Sensor Hubs, extinct so soon?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Smart Sensor Hubs, extinct so soon?

1,049件の閲覧回数
ericstahldavid
Contributor I

The most recent NXP Sensor Catalog (SENSSELECT 2017) lists a catagory of sensors under the heading Smart Sensor Hubs.  The two families of sensors listed are FXLC95000CL and MMA955x.  Both of these families which were first released around 2013-14 (given the press releases I could find) are now at end of life.  Are there any other NXP products that offer an accelerometer embedded with a processor?  Are there any competing part families that made this path non-viable for NXP?

0 件の賞賛
返信
1 返信

993件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi Eric,

Unfortunately, the MMA955xL and the FXLC95000 families were the only devices offering an accelerometer embedded with a processor in the NXP portfolio, so, there are no recommended replacements for these intelligent motion sensing platforms.

 

The recommended replacement for these devices are the stand-alone accelerometers family MMA845x that you can find in the following link: https://www.nxp.com/products/sensors/motion-sensors/accelerometers-for-iot/2g-4g-8g-low-g-14-bit-dig...

 

One suggestion is to use a low power mcu as a sensor hub (like the kinetis KL0x family) and connect a MMA845x accelerometer, suing this combo, you would get a similar system than the FXLC95000 or the MMA955x.


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信