Sensor fusion: commercial support?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sensor fusion: commercial support?

1,871件の閲覧回数
seankelleher
Contributor I

Is commercial support available for the open-source sensor fusion code?  On non-Freescale hardware?
If so, is it subject to purchasing some minimum block of hours or can it be bought on a per-issue basis?


Integration of the code is so far pretty painless, but I want to provide the options to my client.

 

Thanks,
Sean

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,640件の閲覧回数
sinanakman
Senior Contributor III

Sean, if you or your client considers help

from third parties (FSL partners)

please let me know.

Regards

Sinan Akman

0 件の賞賛
返信

1,640件の閲覧回数
michaelestanley
NXP Employee
NXP Employee

Not at this time.

0 件の賞賛
返信

1,640件の閲覧回数
seankelleher
Contributor I

Thanks for the prompt response!

0 件の賞賛
返信