Sensor fusion: commercial support?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sensor fusion: commercial support?

1,100 Views
seankelleher
Contributor I

Is commercial support available for the open-source sensor fusion code?  On non-Freescale hardware?
If so, is it subject to purchasing some minimum block of hours or can it be bought on a per-issue basis?


Integration of the code is so far pretty painless, but I want to provide the options to my client.

 

Thanks,
Sean

Labels (1)
0 Kudos
Reply
3 Replies

869 Views
sinanakman
Senior Contributor III

Sean, if you or your client considers help

from third parties (FSL partners)

please let me know.

Regards

Sinan Akman

0 Kudos
Reply

869 Views
michaelestanley
NXP Employee
NXP Employee

Not at this time.

0 Kudos
Reply

869 Views
seankelleher
Contributor I

Thanks for the prompt response!

0 Kudos
Reply