Sensor Toolbox

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sensor Toolbox

Jump to solution
4,167 Views
sbrack
Contributor I

Hello All,

I have only played around with the functions on the sensor toolbox a little, but is there a way to record the magnetic readings with the program?

Thanks

Sam

Labels (1)
0 Kudos
Reply
1 Solution
3,856 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Sam,

If you are using the RD4247MAG3110 kit, please download and install the E-Compass Sensor Toolbox v6.1.0.1. Then you can start data recording by pressing the Start button in the Data Log frame of the GUI. For more information please refer to Chapter 9 of the E-Compass Sensor Toolbox User Guide.

It is also possible to collect raw data from generic terminal program such as RealTerm using the commands described in the attached document.

I hope it helps.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

View solution in original post

3 Replies
3,856 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Sam,

Could you please specify which evaluation board and Sensor Toolbox version you are using?

Regards,

Tomas

0 Kudos
Reply
3,856 Views
sbrack
Contributor I

I am using a LFSTBUSB interface board with the Sensor Toolbox v4.2.1.20.​ I purchased the RD4247MAG3110 magnetic sensor kit, and I am looking to record some of the magnetic readings using the sensor toolbox. If that is possible.

Thanks

Sam

0 Kudos
Reply
3,857 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Sam,

If you are using the RD4247MAG3110 kit, please download and install the E-Compass Sensor Toolbox v6.1.0.1. Then you can start data recording by pressing the Start button in the Data Log frame of the GUI. For more information please refer to Chapter 9 of the E-Compass Sensor Toolbox User Guide.

It is also possible to collect raw data from generic terminal program such as RealTerm using the commands described in the attached document.

I hope it helps.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.