Sensor Fusion Toolbox Stand alone flash on FRDM-KL25Z failing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Sensor Fusion Toolbox Stand alone flash on FRDM-KL25Z failing

跳至解决方案
1,412 次查看
antoinevanderhe
Contributor I

Hello All,

 

I am trying out the Freescale Sensor Fusion Toolbox (build on 11 september 2015).

 

I only got the following problem when flashing the file: FRDM-KL25Z-V-NED.hex (stand alone) to the MBED drive.

 

I am getting the error BAD EXTENSION FILE (in the fail.txt file)

 

This is on MBED with MBED firmware rev 203. Bootloader version from Pemicro is v111.

 

On which version has it been working/tested? Is there an updated file (hex/bin) available? Or any suggestion what to try more?

 

Thanks in advance!

 

Best regards,

Antoine van der Heijde

标签 (1)
0 项奖励
回复
1 解答
1,204 次查看
michaelestanley
NXP Employee
NXP Employee

Antoine,

The GUI is assuming that KL25Z boards are programmed with OpenSDA V1 by P&E Micro.  That's why they won't work with your MBED-enabled board.

If you reprogram the board to the P&E interface, it should work just fine.

Regards,

Mike

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,205 次查看
michaelestanley
NXP Employee
NXP Employee

Antoine,

The GUI is assuming that KL25Z boards are programmed with OpenSDA V1 by P&E Micro.  That's why they won't work with your MBED-enabled board.

If you reprogram the board to the P&E interface, it should work just fine.

Regards,

Mike

0 项奖励
回复
1,204 次查看
antoinevanderhe
Contributor I

Hi Mike,

Thanks for the quick response!

I did not realized there was a difference between the MSD loaders. It is working very fine now! Thank you.

Best regards,

Antoine

0 项奖励
回复