Hello All,
I am trying out the Freescale Sensor Fusion Toolbox (build on 11 september 2015).
I only got the following problem when flashing the file: FRDM-KL25Z-V-NED.hex (stand alone) to the MBED drive.
I am getting the error BAD EXTENSION FILE (in the fail.txt file)
This is on MBED with MBED firmware rev 203. Bootloader version from Pemicro is v111.
On which version has it been working/tested? Is there an updated file (hex/bin) available? Or any suggestion what to try more?
Thanks in advance!
Best regards,
Antoine van der Heijde
解決済! 解決策の投稿を見る。
Antoine,
The GUI is assuming that KL25Z boards are programmed with OpenSDA V1 by P&E Micro. That's why they won't work with your MBED-enabled board.
If you reprogram the board to the P&E interface, it should work just fine.
Regards,
Mike
Antoine,
The GUI is assuming that KL25Z boards are programmed with OpenSDA V1 by P&E Micro. That's why they won't work with your MBED-enabled board.
If you reprogram the board to the P&E interface, it should work just fine.
Regards,
Mike
Hi Mike,
Thanks for the quick response!
I did not realized there was a difference between the MSD loaders. It is working very fine now! Thank you.
Best regards,
Antoine