Samplerate of FXOS8700 using FRDM-KL26Z_MQXL.hex

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Samplerate of FXOS8700 using FRDM-KL26Z_MQXL.hex

Jump to solution
975 Views
roberto70
Contributor I

What samplerate is FRDM-KL26Z_MQXL.hex that is included with the Freescale Vibration Monitor using for the FXOS8700? Since the software displays frequencies up to 400Hz I assume the maximum possible samplerate of 800Hz is used. Am I right? I'm asking since I see significant differences to my own FXOS8700 implementation on vibrations above 30Hz.

Labels (1)
Tags (2)
0 Kudos
1 Solution
807 Views
JackITB
NXP Employee
NXP Employee

Correct,

Some more details are mentionned in the Help tab, paragraph 5:Sensors

View solution in original post

0 Kudos
3 Replies
807 Views
roberto70
Contributor I

Arrrggh, could have answered that myself. There is a sample each other 1.25ms so the samplerate is 800Hz. Sorry for asking.

0 Kudos
808 Views
JackITB
NXP Employee
NXP Employee

Correct,

Some more details are mentionned in the Help tab, paragraph 5:Sensors

0 Kudos
807 Views
roberto70
Contributor I

Thank you!

0 Kudos