SPI API Definition of TWR-CM3120-EVM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI API Definition of TWR-CM3120-EVM

1,333 Views
sesc
Contributor I

Hello everyone!

I'm interested in the IO-Link capable TWR-CM3120-EVM board and would like to control it's included master stack with a micro controller using the SPI interface. The user guide (found at https://www.nxp.com/docs/en/user-guide/KTTWRCM3120UG.pdf ) mentions that this is possible with the right jumper settings.

Unfortunately, the guide does not specify the API to control it via SPI, nor does it mention if there is a different document describing it.

Is this information available or part of the delivery? I was not able to find information about this on the product page.

Thanks and best regards

Sebastian

0 Kudos
Reply
2 Replies

1,064 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Sebastian,

The IO-Link stack source code as well as the API documentation is available from TEConcept, not from NXP, unfortunately.

 

Please contact them directly through this website:

https://www.teconcept.de/en/content/contact

Best regards,

Tomas

0 Kudos
Reply

1,064 Views
coord_investiga
Contributor I

Hello, i bought  TWR-CM3120-EVM board and i need the software for use it, but the link you gave on past october is not aviable, so could you help me to know where i can get it?.

Thank you in advance.

0 Kudos
Reply