Rotational Position of Automotive Wheel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Rotational Position of Automotive Wheel

1,189 Views
mike_holladay
Contributor I

Can you use an accelerometer to determine when an rotating automotive wheel is pointed toward the ground ?  I assume you have to use a Gyroscope along with the accelerometer but Gyroscopes are expensive and hard to find in the automotive temperature range.  Is it possible with two accelerometers ?

0 Kudos
Reply
5 Replies

1,083 Views
Ben
Senior Contributor I

Mike, you can use accelerometer, but you need a sensor defined as inclinometer.

See for example the Analog ADIS16210 (with SPI communication)

BR

Ben

0 Kudos
Reply

1,082 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Mike,

Could you please elaborate on your application/use case? I do not quite understand it now.

If you needed a gyroscope, you would have to look at other manufacturers as there are not any AEC-Q100 qualified gyroscopes currently in NXP portfolio, unfortunately.

Best regards,

Tomas  

PS: If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.

0 Kudos
Reply

1,083 Views
mike_holladay
Contributor I

Tomas

It is actually an Ag tractor application. Just need a sensor to determine

when a certain spot on the Ag tire rim is pointed toward the ground.

The environment and temperature in this application is such that the MEMS

sensor should at least operate up to and calibrated for +105C. AEC-Q100

may not be a hard requirement.

Mike

On Tue, Mar 26, 2019 at 3:56 AM TomasVaverka <admin@community.nxp.com>

0 Kudos
Reply

1,083 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Mike,

I have discussed it with colleagues from our TPMS Apps Team and they developed a project in which the TPMS monitors the angular position and transmits a frame when it reaches a pre-defined angle (the angle is defined by the user).

To do that only one accelerometer measuring the radial acceleration is required. In the TPMS this corresponds to the X-axis.

Image 01.jpg

The project and related documentation can be downloaded from:

https://www.nxp.com/support/developer-resources/software-development-tools/sensor-developer-resource...

pastedImage_5.png

If you have any other questions, please let me know.

Best regards,

Tomas

0 Kudos
Reply

1,083 Views
mike_holladay
Contributor I

Tomas

Ok, I will check it out, thanks for the info.

Mike

On Wed, Mar 27, 2019 at 7:25 AM TomasVaverka <admin@community.nxp.com>

0 Kudos
Reply