Reflow oven profile for sensor MPXV5004DP.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reflow oven profile for sensor MPXV5004DP.

Jump to solution
1,234 Views
dariosena
Contributor I

Hi, where can i find the tipical reflow oven profile for sensor MPXV5004DP. This information is not in the datasheet. We have a high rate of fails and suspect the part is sensitive to a normal ROHS profil. Thank you

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,056 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Dario,

Please refer to our AN3150 – “Soldering Recommendations for Pressure Sensor Devices”. The maximum peak temperature during the soldering process should not exceed 245°C for 30 seconds maximum duration as shown on this website.

I hope it helps.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

View solution in original post

0 Kudos
Reply
2 Replies
1,057 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Dario,

Please refer to our AN3150 – “Soldering Recommendations for Pressure Sensor Devices”. The maximum peak temperature during the soldering process should not exceed 245°C for 30 seconds maximum duration as shown on this website.

I hope it helps.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

0 Kudos
Reply
1,056 Views
dariosena
Contributor I

Thank you so much Tomas. is exactly what I'm looking for.

0 Kudos
Reply