Quality report of MPX2300DT1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Quality report of MPX2300DT1

2,026 Views
raymondto
Contributor I

Hello, I am looking for packaging quality report of MPX2300DT1. (such as MSL, HAST, etc). Where can I find it?

Labels (1)
Tags (3)
0 Kudos
Reply
3 Replies

1,783 Views
Joshevelle
Senior Contributor I

Hello Raymond,

Thanks for using our community.

The MSL is the moisture level that an electronic device can stand without popping up in the soldering process (moisture expansion). All the pressure sensors like the MPX2300 has at least one pressure port. There is no MSL rating for ported devices since moisture expansion would not affect them.

As per the Highly Accelerated Stress Tests, I would like refer to the "Quality and Reliability" at DL200 Data Library at pages 1-3 to 1-14. Specifically page 1-8 "Accelerated Life Testing"

http://cache.freescale.com/files/sensors/doc/data_lib/DL200.pdf

(Please note that the size of the book will require ~25MB).

Hope it helps!

Josh

1,783 Views
raymondto
Contributor I

Hello Josh,

Thanks for your reply. According to DL200, do you mean that MPX2300DT1 already passed page 1-11 class 1 and page 1-17 conditions? Or I can obtain an individual test report on your database?

With much appreciation!

Raymond

0 Kudos
Reply

1,783 Views
Joshevelle
Senior Contributor I

Hello Raymond,

The pressure sensors are qualified by family, DL200 covers all of our pressure sensors. Unfortunately we do not have the specific data for the  MPX2300DT1.


Josh

0 Kudos
Reply