Quality report of MPX2300DT1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Quality report of MPX2300DT1

1,885 次查看
raymondto
Contributor I

Hello, I am looking for packaging quality report of MPX2300DT1. (such as MSL, HAST, etc). Where can I find it?

标签 (1)
标记 (3)
0 项奖励
回复
3 回复数

1,642 次查看
Joshevelle
Senior Contributor I

Hello Raymond,

Thanks for using our community.

The MSL is the moisture level that an electronic device can stand without popping up in the soldering process (moisture expansion). All the pressure sensors like the MPX2300 has at least one pressure port. There is no MSL rating for ported devices since moisture expansion would not affect them.

As per the Highly Accelerated Stress Tests, I would like refer to the "Quality and Reliability" at DL200 Data Library at pages 1-3 to 1-14. Specifically page 1-8 "Accelerated Life Testing"

http://cache.freescale.com/files/sensors/doc/data_lib/DL200.pdf

(Please note that the size of the book will require ~25MB).

Hope it helps!

Josh

1,642 次查看
raymondto
Contributor I

Hello Josh,

Thanks for your reply. According to DL200, do you mean that MPX2300DT1 already passed page 1-11 class 1 and page 1-17 conditions? Or I can obtain an individual test report on your database?

With much appreciation!

Raymond

0 项奖励
回复

1,642 次查看
Joshevelle
Senior Contributor I

Hello Raymond,

The pressure sensors are qualified by family, DL200 covers all of our pressure sensors. Unfortunately we do not have the specific data for the  MPX2300DT1.


Josh

0 项奖励
回复