QN9080-DK Temperature

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

QN9080-DK Temperature

1,045 次查看
hbburnha
Contributor I

This may be a dumb question, but does the QN9080-DK have a temperature sensor on the board, or does it only receive temperature measurements via BLE?

0 项奖励
回复
1 回复

1,034 次查看
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi, Hayden,

QN9080 integrates a temperature sensor that is connected to one internal dedicated ADC channel as it is only for device internal temperature measurement.

Please, take a look at the QN908x Data Sheet, Chapter 8.17.2: Temperature sensor; and the QN908x ADC Configuration Guide, Chapter 7: Temperature measurement.

Also, you can find an example of ADC driver usage in addition with the temperature sensor inside the SDK examples (SDK examples > driver_examples > adc > temperature).

Regards,
Eduardo.

0 项奖励
回复