Dear Team,
My customer is looking for a pressure sensor with a measuring range of 0 - 10 kPa (output interface could be I2C or Analog) but will have a tolerance of pressure up to 250 kPa so that the sensor will not fail.
Also, the sensor should support direct contact with wet (water) media in the pressure sensor nozzle input (water as pressure media)?
Please suggest a suitable solution/sensor, Thanks in advance.
Kind Regards,
Dear Shai,
Unfortunately none of our currently available 10 kPa pressure sensors are capable to withstand a pressure up to 250 kPa and direct contact with wet (water) media.
Best regards,
Tomas