Pressure sensor questions

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Pressure sensor questions

1,803 次查看
kevinroach
Contributor I

I am looking for a pressure sensor that would be effected by the weather. Does NXP make any?

I am reading flow pressure through a two stroke engine needle valve and want to ajust flow with weather effecting adjustment.

I know there is some Sunx modules that are used in semiconductor manufacturing but don't want to go that route.

0 项奖励
回复
3 回复数

1,537 次查看
david_diaz
NXP Employee
NXP Employee

Hello Kevin,

I hope all is great with you.

What do you mean with effected by the weather?

As a first option, I would like to recommend the MPL3115A2 device.

The MPL3115A2 is an absolute pressure sensor with an I2C digital interface. The compensated pressure output can then be converted to altitude, utilizing the formula stated in Section 8.1.3 "Pressure/altitude" provided in meters.

So, the device can be used for High-accuracy altimetry and barometry.

Please let me know if this information is useful for you.

Regards,

David

0 项奖励
回复

1,537 次查看
kevinroach
Contributor I

David,

Do you carry on pressure sensor that are compatible with water? I work on

dialysis machines and have to calibrate water pressures.

The sensor would have to withstand getting water in it and have an output

for a micropressor.

Thanks,

Kevin

0 项奖励
回复

1,537 次查看
darioarias
NXP Employee
NXP Employee

Hi Kevin,

The sensors we have are only guaranteed for use in dry and clean air conditions, we don't have any sensor that work specifically in water. However, with some special technique (air column) is possible to measure this pressure. 

The application note: Media compatibility for pressure sensors gives detail in some test conducted for this pressure sensors in different media and the air column technique.

Darío

0 项奖励
回复