Pressure media for MPXHZ6400AC6T1?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Pressure media for MPXHZ6400AC6T1?

ソリューションへジャンプ
1,008件の閲覧回数
vasilijvasechki
Contributor I

Hello. Can be used sea water and river water as the pressure media for MPXHZ6400AC6T1 sensor?

ラベル(1)
0 件の賞賛
返信
1 解決策
869件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Vasilij,

Yes, but our recommendation is to separate the media from the sensor by a column of clean, dry air as shown in the AN3728. Some vaporization of the media will occur in the air column, but for most applications the Media Resistant gel provides an adequate protection.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
870件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Vasilij,

Yes, but our recommendation is to separate the media from the sensor by a column of clean, dry air as shown in the AN3728. Some vaporization of the media will occur in the air column, but for most applications the Media Resistant gel provides an adequate protection.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

0 件の賞賛
返信