Pressure media for MPXHZ6400AC6T1?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pressure media for MPXHZ6400AC6T1?

Jump to solution
627 Views
vasilijvasechki
Contributor I

Hello. Can be used sea water and river water as the pressure media for MPXHZ6400AC6T1 sensor?

Labels (1)
0 Kudos
Reply
1 Solution
488 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Vasilij,

Yes, but our recommendation is to separate the media from the sensor by a column of clean, dry air as shown in the AN3728. Some vaporization of the media will occur in the air column, but for most applications the Media Resistant gel provides an adequate protection.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

View solution in original post

0 Kudos
Reply
1 Reply
489 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Vasilij,

Yes, but our recommendation is to separate the media from the sensor by a column of clean, dry air as shown in the AN3728. Some vaporization of the media will occur in the air column, but for most applications the Media Resistant gel provides an adequate protection.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

0 Kudos
Reply