Pavel, we have not ported to FRDM-K82F, but K64F is supported for both CodeWarrior and KDS. And the K22F is supported for KDS only. There should be no reason you could not port to the new K82F however. From a hardware perspective, It certainly has the flash and RAM complement required. I haven't done a detailed analysis of the shield connections, but expect it will be compatible with the FRDM-FXS-MULT2-B board, as well as the FRDM-FXS_AGMP01. The one thing I don't know (perhaps someone from the MCU division can chime in?) is whether there is Processor Expert support for it. The current sensor fusion kit (V5.00) utilizes LDDs for the serial ports. We don't have a full port to KDSK yet.
Regards,
Mike