Please explain what you mean by the datasheet term "sensitivity accuracy" for the 8542Q xtrinisc accelerometer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Please explain what you mean by the datasheet term "sensitivity accuracy" for the 8542Q xtrinisc accelerometer

842 Views
dylanpfeifer
Contributor I

Hi Freescale--

We do not understand what you mean by the term "sensitivity accuracy" in the parameters for the Xtrinsic 8452Q accelerometer, according to the datasheet.  How does this number apply to the sensitivity and scale?

Thanks,

Dylan

Labels (1)
0 Kudos
Reply
1 Reply

696 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Dylan,

Sensitivity Accuracy describes the range of sensitivities of a large population of sensors. In other words, it is possible that for one sensor the sensitivity is more closely to the typical value but for other it might be somewhere in the range of So +/- So x 0.0264.

That being said, as a result of thermal and mechanical stresses during the soldering process, re-calibration is recommended for applications requiring higher accuracy. This involves placing the final product at multiple orientations and calculating 12 additional new calibration parameters which should then be stored in non volatile memory and applied by an external uC. We have an application note AN4399 and example code illustrating how to do this. We recommend the 12 point algorithm that corrects for a 3x3 gain matrix and 3x1 offset vector.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

0 Kudos
Reply