Part no. MPXA4115AC6U question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Part no. MPXA4115AC6U question

1,171 Views
demilaluan
Contributor I

Hi there!,

Please confirm if this part no. can be washed or not.

Thanks,

Demi

NOTICE: The information contained in this email is intended for the individual or entity above. This email is protected by the Electronic Communications Privacy Act, 18 U.S.C. Sections 2510-2521. In addition to the foregoing, nothing in this message should be interpreted as a digital or electronic signature that can be used to form, execute, document, agree to, enter into, accept or authenticate a document and the recipient should not rely on it for any such purpose. If you are not the intended recipient, please do not read, copy, use, forward or disclose this communication to others. Also, please notify the sender by replying to this message and then delete this message from your system.

0 Kudos
Reply
1 Reply

1,096 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Demi,

Cleaning/Wash process is different with pressure sensors because the diaphragm (gel) inside the device.

Our Quality Engineers do not recommend to clean this devices. However, if you want to clean the device, you can only clean it on the outside, with some paper or swab with alcohol.

 

Any cleaner that that enters the pressure sensor opening may have adverse effects on the device.

So, sealing the access hole on the part with kapton tape is absolutely recommended. You can plug also the sensors with a cap before cleaning.

Caps can be found via stockcap

 

Ultrasonic cleaning is not recommended as the frequencies can damage wire bond interconnections.

 

Many customers have gone to no clean operations or spray clean in a direction where the spray is not directly going into the sensor hole.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply