New MPX5100DP no Vout

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

New MPX5100DP no Vout

ソリューションへジャンプ
4,594件の閲覧回数
max-g
Contributor I

I've got a new MPX5100DP, which I connected to an Arduino, as follows:

pin 1: Vout to A0 on Arduino (analog in)

pin 2: ground on Arduino ground

pin 3: Vcc on Arduino 5V

This simple code:

#define MPX5100_PIN A0 // MPX5100DP sensor pin

void setup() {

  pinMode(MPX5100_PIN, INPUT);

  Serial.begin(9600);

}

void loop() {

  unsigned int pressureSensorValue;

  pressureSensorValue = analogRead(MPX5100_PIN);

  Serial.print("Pressure value.....: ");

  Serial.println(pressureSensorValue);

  delay(2000);

}

... does not produce any other value than 1017.

How can I check, whether this sensor is actually functioning?

タグ(2)
0 件の賞賛
返信
1 解決策
3,713件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Max,

Yes, as Anthony suggested, try to force some air into P1, e.g. using your mouth and see if the voltage goes up. Also check the output voltage when no pressure is applied, it should produce about 0.2V (0.088V - 0.313V).

Regards,

Tomas

元の投稿で解決策を見る

4 返答(返信)
3,713件の閲覧回数
max-g
Contributor I

Yes, hardware or software :smileyhappy:

Thank you guys! I put a poti on the same analogue input and it worked; assuming the sensor is dead... and ordered a new one.

I had an air pump connected to either port and nothing changed on the analogue port.

What a great idea to use a Volt meter (embarrassed)... and guess what? ... it works! 185mV.

One port the voltage goes down, the other it goes up.

Which one is the port I should use as in put wanting to measure a water level (via tube dangling in water tank)? -- The one where the voltage goes up?!

I am lost for words, or rather an explanation... wired it up and ran the sketch... it works as it should... :-S

0 件の賞賛
返信
3,713件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Max,

Glad to hear our suggestions have been helpful.

Yes, use the  P1 port and leave the P2 port open, since the MPX5100DP is designed to be used under P1>P2 condition.

Regards,

Tomas

0 件の賞賛
返信
3,713件の閲覧回数
anthonyduhamel
NXP Employee
NXP Employee

Hi Max,

It an be a software problem or a sensor issue. I suggest you to use a voltmeter to measure the MPX5100 outout voltage. You can blow/draw into the sensor and check if the voltage has changed.

Anthony

3,714件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Max,

Yes, as Anthony suggested, try to force some air into P1, e.g. using your mouth and see if the voltage goes up. Also check the output voltage when no pressure is applied, it should produce about 0.2V (0.088V - 0.313V).

Regards,

Tomas