Need help in selecting a Sensor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need help in selecting a Sensor

777 Views
radheshpulimutt
Contributor I

Hello, For my Mater thesis I am developing an Interactive Globe, for which I require a sensor which can sense TOUCH. The user will be touching a continent and this should result in stating the respective name of the continent. The problem I am facing is that the user won't be touching the sensor directly. Can anybody suggest a sensor for this application???

0 Kudos
Reply
1 Reply

673 Views
darioarias
NXP Employee
NXP Employee

Hi Radhesh,

The portfolio of low-power touch sensors use the human body as one of the capacitive plates of an electrical circuit.  Capacitive sensors can also switch without contact due to proximity sensing or used with external plates connected to the device. I think this type of sensor are suitable for your application where the external plate is shaped as a continent. The sensors we have are, PCF8883 and PCF8885.

Hope you found them useful

Darío

0 Kudos
Reply