NTM88 maximum sensor samples per second via SPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NTM88 maximum sensor samples per second via SPI

3,229 Views
martijn-VB
Contributor I

Hello,

We're interested in using the NTM88 in one of our applications.

What is the maximum samples per second we can get from the pressure sensor and accelerometer? And what is the maximum response time of both sensors? (I couldn't find it in the datasheet, I might have overlooked it...)

With kind regards,
Martijn

Labels (1)
0 Kudos
Reply
5 Replies

3,003 Views
martijn-VB
Contributor I

Can anyone point me in the right direction?
I'm not looking for SPI information but information about the actual sensing elements in the chip.

How fast is the pressure sensor and accelerometer?
Does the pressure and accelero reading from the sensor update with 1Hz or with 1000Hz?

And what is the reponsetime of the sensors?
If the pressure or accelerration in the vehicle change very fast (ms range), how fast will the sensor reading out of the sensor change?

0 Kudos
Reply

2,977 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

Sorry for not responding earlier.

Please see Implementing Wired Communication with the NTM88 

 

0 Kudos
Reply

3,149 Views
martijn-VB
Contributor I

Hi ErikaC,

I'm sorry, I've not formulated my question clear enough.
I was not looking for the SPI specific information but sensor specific.

How fast is the pressure sensor and accelerometer?
Does the pressure and accelero reading from the sensor update with 1Hz or with 1000Hz?

And what is the reponsetime of the sensors?
If the pressure or accelerration in the vehicle change very fast (ms range), how fast will the sensor reading out of the sensor change?

With kind regards,
Martijn

0 Kudos
Reply

3,102 Views
martijn-VB
Contributor I

@ErikaCAny more information on this?

0 Kudos
Reply

3,200 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello, please refer to the SPI section of the NTM88 manual for information on the protocol and frame format supported by the NTM88 UM11227 section 10.18, and the attached document.

Hope this helps.

 

 

0 Kudos
Reply