NTM88: changing RF transmit power(434MHz)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NTM88: changing RF transmit power(434MHz)

Jump to solution
314 Views
ankit2631
Contributor II

Currently i am using NTM88 stater project example and i want to reduce the TX power of RF 434MHz, which function is used to change the default TX power.

0 Kudos
Reply
1 Solution
303 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Ankit,

There is a function called TPMS_RF_DYNAMIC_POWER that is used to change the RF power setting. For more information please refer to the UM11145 (NTM88 Firmware Library User Guide), chapter 3.2.29.

BR, Tomas

View solution in original post

0 Kudos
Reply
1 Reply
304 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Ankit,

There is a function called TPMS_RF_DYNAMIC_POWER that is used to change the RF power setting. For more information please refer to the UM11145 (NTM88 Firmware Library User Guide), chapter 3.2.29.

BR, Tomas

0 Kudos
Reply