NTM88 acceleration values on x-axis varying from IC to IC in resting state and in same position

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NTM88 acceleration values on x-axis varying from IC to IC in resting state and in same position

Jump to solution
664 Views
ankit2631
Contributor II

 for example: resting state acceleration value of x axis in 'gu16CompAccelX' register of one NTM88 is 504,for second NTM88 is 524,and 3rd NTM88 is 511. is this normal? and have can i solve this if this is not normal. And i am using the example project code NTM88_GenFSK_Beacons. i am using this values of gu16CompAccelX register to check if the vehicle is moving or not.

Tags (2)
0 Kudos
Reply
1 Solution
645 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Ankit, 

There are tolerances indicated in the measurement characteristics section in the datasheet, taking into account all sources of errors (offset error, sensitivity error, error due to temperature on the temperature range indicated and aging).

There should be a significant difference in acceleration values when a vehicle is moving or stationary.

Best regards,

Tomas

View solution in original post

0 Kudos
Reply
1 Reply
646 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Ankit, 

There are tolerances indicated in the measurement characteristics section in the datasheet, taking into account all sources of errors (offset error, sensitivity error, error due to temperature on the temperature range indicated and aging).

There should be a significant difference in acceleration values when a vehicle is moving or stationary.

Best regards,

Tomas

0 Kudos
Reply