NTM88 Sensor Data?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

NTM88 Sensor Data?

跳至解决方案
3,369 次查看
Markel
Contributor I

Hi,

We are reading the NTM88 through SPI interface using CC2640R2F(BLE). Initial details are in this post.

https://community.nxp.com/t5/Sensors/Not-able-to-get-correct-sensor-data-from-NTM88/td-p/1453940

We are using the GenFSK_Beacons_Demo_NTM88_KW38 as reference.

When I debug the "NTM88_GenFSK_Beacons", The TPMS ID and sensor data are saved in this array.

/* Fill the data array*/
gau8DataArray[u8index++] = gau8TpmsId[0];
gau8DataArray[u8index++] = gau8TpmsId[1];
gau8DataArray[u8index++] = gau8TpmsId[2];
gau8DataArray[u8index++] = gau8TpmsId[3];
gau8DataArray[u8index++] = gau8TpmsId[4];
gau8DataArray[u8index++] = gau8TpmsId[5];
gau8DataArray[u8index++] = (UINT8)(gu16CompPressure >> 8);
gau8DataArray[u8index++] = (UINT8)(gu16CompPressure);
gau8DataArray[u8index++] = (UINT8)(gu16CompAccelZ >> 8);
gau8DataArray[u8index++] = (UINT8)(gu16CompAccelZ);
gau8DataArray[u8index++] = (UINT8)(gu16CompAccelX >> 8);
gau8DataArray[u8index++] = (UINT8)(gu16CompAccelX);
gau8DataArray[u8index++] = gu8CompVolt;
gau8DataArray[u8index++] = gu8CompTemp;

From debugging this is the sensor data at NTM88.

sensor data.jpg

This is the same data we receive at CC2640R2(BLE) through SPI interface. I print the output to Tera Term.

CC2640R2F sensor data.jpg

Why is the voltage and temperature reading from NTM88 both 1? Also are the compensated pressure, acc z and accx are correct. Sorry the ACC Y above is supposed to be ACC X.

Also how do I properly convert the raw sensor data in proper units of psi, g, volts, Celsius.

Regards,

Markel

0 项奖励
回复
1 解答
3,354 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Markel,

The SPI communication seems to go well: the data stored in the array is exactly the same data read on the host MCU side.

The fact that all sensor data is underflow or overflow, and that the TPMS ID is all 0xFF, indicates that the trim section (from 0xFD40 to 0xFDFF) has been erased. There is no solution to recover the chip in that case as the trim coefficients are unique to each device (so they cannot be copied from one device to another).

The trim section is erased if a mass erase is performed, for example when clicking on the button “Erase Whole Device” with Flash Programmer Tool (button with a red cross on the screenshot below, extracted from CW user guide):

1.png

The trim coefficients only impact the sensor measurements, the rest of the features are still functional. So the chip can be used to work on communication, handshaking etc. But to get valid sensor measurements, a new chip will be needed.

More information on sensor measurements can be found in the app note below:

https://www.nxp.com/webapp/Download?colCode=AN13614

Best regards,

Tomas

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,185 次查看
Carter4787
Contributor I

Thanks for the step by step tutorial. Works like a charm! The solution worked for me thanks to the community and the members for the solution.  MGS.Marriott.com

0 项奖励
回复
3,355 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Markel,

The SPI communication seems to go well: the data stored in the array is exactly the same data read on the host MCU side.

The fact that all sensor data is underflow or overflow, and that the TPMS ID is all 0xFF, indicates that the trim section (from 0xFD40 to 0xFDFF) has been erased. There is no solution to recover the chip in that case as the trim coefficients are unique to each device (so they cannot be copied from one device to another).

The trim section is erased if a mass erase is performed, for example when clicking on the button “Erase Whole Device” with Flash Programmer Tool (button with a red cross on the screenshot below, extracted from CW user guide):

1.png

The trim coefficients only impact the sensor measurements, the rest of the features are still functional. So the chip can be used to work on communication, handshaking etc. But to get valid sensor measurements, a new chip will be needed.

More information on sensor measurements can be found in the app note below:

https://www.nxp.com/webapp/Download?colCode=AN13614

Best regards,

Tomas

0 项奖励
回复
2,769 次查看
Joey_Legaspi
Contributor I

Hello Tomas,

Is there a way to write semi-sane coefficients into it? 

Just so we can read somewhat realistic values from the sensor for development purposes (they don't have to be accurate).

BR,
Joey

0 项奖励
回复
3,346 次查看
Markel
Contributor I

Hi Tomas,

I did click the Erase Whole Device 1x. There is nothing in the user's guide that I have read that says do not click the Erase Whole Device.

Regards,

Markel

0 项奖励
回复