NTM88 | SPI Not working as expected

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NTM88 | SPI Not working as expected

1,329件の閲覧回数
shai_b
Senior Contributor II

Dear Team,

My customer is working with our NTM88 sensor and having an issue communicating with his MCU via SPI.

according to the customer while he was overviewing all our documents he notice a few mismatched in information.

for example, the NTM88 Firmware Library User Guide (UM11145) explains that the sensors use PTA0 and PTA1 for CLK and DATA and the example code of the NTM88+KW38 example guide shows a different setup of pins which is confusing.

So the customer chooses the stick with the example code of NTM88+KW38 BLE Beacons as a baseline for his code and his setup is NTM88+Silab (BLE) as below: 

NTM88_MCU.png

The customer's question is to understand why the SPI communication is not working, the customer has noticed the KBI interrupt works but he doesn't see any data from the sensor.

Please advise back what could be wrong ?

 

Waiting for your kind feedback, many thanks.

Regards,

Shai

ラベル(3)
タグ(1)
0 件の賞賛
返信
1 返信

1,322件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Shai,

I hope all is great with you. Thank you for using the NXP communities.

Please review the file that I will send you by email. Configuration of the mapping between GPIOs and SPI/I2C functions are shown in Figure 4.

I hope this information helps.

Regards,

David

0 件の賞賛
返信