Measure vacuum pressure via MPXV6115V

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Measure vacuum pressure via MPXV6115V

Jump to solution
1,800 Views
LORDSUN1
Contributor I

When I used the Arduino board and the MPXV6115V sensor to measure the vacuum pressure, the output from the Vout pin shows the value around 900, which should be 1023 (due to the ADC function of the Arduino board).

I am not sure why this happens. Is it normal for the vacuum pressure sensor?

0 Kudos
1 Solution
1,792 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Xiyang,

 

Which Arduino board are you actually using and what is the voltage (in Volts) on the Vout pin? You should see something around 4.6V with no pressure applied and 5.0V supply voltage:

 

Capture.JPG

 

Best regards,

Tomas

   

View solution in original post

0 Kudos
2 Replies
1,793 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Xiyang,

 

Which Arduino board are you actually using and what is the voltage (in Volts) on the Vout pin? You should see something around 4.6V with no pressure applied and 5.0V supply voltage:

 

Capture.JPG

 

Best regards,

Tomas

   

0 Kudos
1,786 Views
LORDSUN1
Contributor I

Thanks for your kind notification.

Yes, you're right. The arduino board I used is the Arduino Mega 2560, the output from the pressure sensor is around 900, due to the Analog-digital-conversion, thus the output voltage should be 900/1023*5 V, around 4.5V.

0 Kudos