May I use MVPXV5050DP pressure sensor to messure pressure in water?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

May I use MVPXV5050DP pressure sensor to messure pressure in water?

923 Views
omarpugliesi
Contributor I

I need to messure pressure in water, and like I made a big pressure device with MVPXV5050DP sensors, I would lie to know if would be possible to use this device to messure pressure in water condition

Labels (1)
0 Kudos
Reply
1 Reply

782 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Omar.

We do not recommend the MPXV5050DP to become in direct contact with any kind of liquid substance or corrosive gases which would damage the gel and cause the sensor to become out of specification.

 

The strain gauge and the electronic circuitry for calibration and compensation are protected by a nitride layer but the aluminum bonding pads which provide electrical connections between the leadframe and the gauge are not protected, in order to make the bonding feasible. The complete die is also protected with a silicone gel. This gel is not fully hermetic, although we use much better gel for our newer types of pressure sensors, water or any other fluid can penetrate the gel and can reach the die. When the sensor die is in contact with water e.g., oxydoreduction reactions between Al/Al3+ and water start as soon as the sensor is biased. After some working hours, or maybe days, the aluminum pad of the supply pin is definitely destroyed, so that an open circuit on the Vcc pin occurs. This is an aluminum corrosion phenomena. But the corrosion phenomena is stopped when the sensor supply voltage is switched off. There are also some other failure causes like galvanic corrosion, but the Mean Time To Failure (MTTF) due to these other causes much longer than the MTTF caused by electrocorrosion of the Vcc pad. Therefore electrocorrosion is the major failure cause, and they are permanent.

 

However, as you may know, our products are used in washing machine applications, which would expose the gel to a humid environment. In these applications, the device is located at the top of a measurement tube - so water level is indirectly measured through the water pushing a trapped air column up to the sensor. As you can see, the sensor does not have a direct contact with water, but is separated by the air column.

                                   

AN3728: Media Compatibility for IPS PRT Pressure Sensors

https://www.nxp.com/docs/en/application-note/AN3728.pdf 

Best regards,

Tomas

0 Kudos
Reply