Hello! I already using MPXV7025GC6U-ND.
Can I connect silicon tube to MPXV7025GC6U for differential pressure measurement( -187~+187mmHg)?
If MPXV7025GC6U is not proper model for connecting gas silicon tube,
can you recommend proper model?
Thanks.
Hello Sangwhook,
yes, the MPXV7025G is suitable for measuring the negative and positive pressure from -25kPa to +25kPa and can withstand pressure up to 200kPa without damage. For measuring the gas or other compounds, I would recommend you MPVZ7025GC6U, where a Media Resistive Gel covers the die and wire bonds, instead of standard flourosilicone gel. Please find an AN3728 attached, where Media Compatibility with our sensors is discussed.
With Best Regards,
Jozef