MPXV5100DP异常损坏直通(MPXV5100DP abnormally damaged passthrough)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPXV5100DP异常损坏直通(MPXV5100DP abnormally damaged passthrough)

924 Views
jiaming
Contributor I

我用MPXV5100DP这一款型号的压力传感器检测负压,负压最大不超过一个大气压。但是部分仪器工作一段时间后发现传感器P1和P2两个口直通了,无法再检测到压力值。P1正压口我接的是大气压,P2负压口我接的是真空泵。

(I use the pressure sensor of this model MPXV5100DP to detect negative pressure, and the maximum negative pressure does not exceed one atmosphere. However, after some instruments work for a period of time, it is found that the two ports of sensor P1 and P2 are connected directly, and the pressure value can no longer be detected. The positive pressure port of P1 is connected to atmospheric pressure, and the negative pressure port of P2 is connected to a vacuum pump.)

0 Kudos
Reply
1 Reply

916 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

The MPXV5100DP is a standard differential pressure sensor. Perhaps for your application would be better a negative gauge pressure sensor such as the MPXV6115V6U which measures how much the pressure is below local atmospheric pressure. This device is designed to measure „vacuum“ from 0kPa (atmospheric pressure applied to the sensor pressure port) down to -115kPa.

Best regards,

Tomas

0 Kudos
Reply