MPXV5050GP - Pin functions and package

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPXV5050GP - Pin functions and package

1,637件の閲覧回数
prathameshdhanp
Contributor I

Hi,

I am thinking of using MPXV5050GP and the datasheet says that it is of SOP-8 package. But the dimensions are quite different than the usual SOP-8 package. Also, the pin functions are based on style 1 and style 2, but the datasheet doesn't say which one applies to MPXV5050GP. Can anyone throw light on this please?

Thank you.Sensors

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,102件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi Prathamesh Dhanpalwar,

Package used in the MPXV5050GP is a SOP-8 with a case no. 1369-01, package dimensions of this device can be found here.

As stated in Document DOC-97353, the difference between style 1 and style 2 in the package dimensions is due to the two main families of pressure sensors Freescale offers.

Style 1 is usually applicable for all MPXx10, MPXx53 and MPXx2000-series SOP Type package pressure sensors featuring differential outputs.

Style 2 is applicable for all MPXx4000-series, MPXx5000-series, MPXx6000-series, MPXx7000-series integrated devices in surface mount packages featuring single ended outputs.

So for the case of the MPXV5050GP, case no. 1369-01, you should use Style 2:

Pin 1: N/C

Pin 2: Vs

Pin3: GND

Pin 4: Vout

Pin 5: N/C

Pin 6: N/C

Pin 7: N/C

Pin 8: N/C

Additionally, you can find a 3D Step design for this package here.


Have a great day,
Jose Reyes

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信